AXIS#.OPMODE
Description
AXIS#.OPMODE specifies the operation mode of the drive. You must also use AXIS#.CMDSOURCE to set the source of the command to the drive.
The operation mode values can be set as follows:
|
Mode |
Description |
|---|---|
|
0 |
Current (torque |
|
1 |
Velocity operation mode |
|
2 |
Position operation mode |
AXIS#.OPMODE can be changed while the drive is enabled or disabled. If you are using the terminal to change the operation mode, then it is recommended that you disable the drive before changing the operation mode. If you change the operation mode from the terminal while the drive is enabled, the system may experience a step change in demand.
Example
Set the source of the command to a TCP/IP channel and the desired operation mode to velocity:
-->CMDSOURCE 0
-->OPMODE 1
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
0 to 2 |
|
Default Value |
0 |
|
Data Type |
Integer |
|
Stored in Non Volatile Memory |
Yes |
Gantry Mode
If the Axis is in Gantry Mode (CMDSOURCE = 4), then this opmode setting will have no effect until the CMDSOURCE is set to something other than 4 – Gantry.
Variants Supported
All variants are supported.
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
AXIS1.OPMODE | 0x5000 | 0x5 | USINT | - | - | RW | False |
| AXIS2.OPMODE | 0x5100 | 0x5 | USINT | - | - | RW | False |